AXIS#.SAFEPARAM.SBT.TORQUEDURATION

Description

Indicates the duration in milliseconds that current is applied to the motor with the brake applied during the Safe Brake Test (SBT).

 

Parameters Editor with the Torque Duration row circled

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

ms

Range

500 ms to 60000 ms

Default Value

500 ms

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SBT.TORQUEDURATION

3157h

06h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SBT.TORQUEDURATION

3257h

06h

Unsigned16

-

-

Read/Write

No